hello world program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hello world program

1,770 Views
rashmikj
Contributor III

Hi, 

I am using LS1046ardb Kit. Iam able to compile a sample hello world example in Ubuntu 18 using cross compiler aarch64-linux-gnu-gcc and tranfer the object files to the kit using serial port kermit. When i run the file in the kit , nothing get displayed on the kit console. how do i print messages in the console.

Kindly help.

Labels (1)
0 Kudos
Reply
3 Replies

1,764 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try whether the attached elf file can be executed to print "Hello World" successfully on your target board.

1. On your host PC create test.c as the following.

#include <stdio.h>

void main()
{
printf("Hello World!");
}

2. Cross compile test.c.

aarch64-linux-gnu-gcc test.c -o test.out

3. Copy test.out to ls1046ardb target board.

root@TinyDistro ~]$ ./test.out
Hello World![root@TinyDistro ~]

0 Kudos
Reply

1,755 Views
rashmikj
Contributor III

Hi,

Thank for the solution. How to transfer the file to the kit? Which protocol is supported?

0 Kudos
Reply

1,741 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could copy the file to USB storage device. Or setting up networking environment, and use "scp" command to copy the file from the PC to the target board.

0 Kudos
Reply