flex-builder build failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flex-builder build failure

3,112件の閲覧回数
penman
Contributor II

I am building flexbuilder_lsdk on Ubuntu 18.04 with:

flex-builder -i clean

flex-builder -i clean-rfs

flex-builder -i repo-update

flex-builder -m ls1046ardb -a arm64

and the build fails with the message:

installing for second-stage ...
I: Keyring file not available at /usr/share/keyrings/ubuntu-archive-keyring.gpg; switching to https mirror https://deb.debian.org/debian
I: Installing core packages...
W: Failure trying to run:  dpkg --force-depends --install /var/cache/apt/archives/base-passwd_3.5.44_arm64.deb
W: See //debootstrap/debootstrap.log for details (possibly the package /var/cache/apt/archives/base-passwd_3.5.44_arm64.deb is at fault)

Here is the output of the debootstrap.log

$ cat build/rfs/rootfs_lsdk1906_LS_arm64_main/debootstrap/debootstrap.log
gpgv: Signature made Thu Apr 26 18:38:40 2018 CDT
gpgv:                using RSA key 3B4FE6ACC0B21F32
gpgv: Good signature from "Ubuntu Archive Automatic Signing Key (2012) <[email protected]>"
dpkg: warning: parsing file '/var/lib/dpkg/status' near line 5 package 'dpkg':
 missing description
dpkg: warning: parsing file '/var/lib/dpkg/status' near line 5 package 'dpkg':
 missing architecture
Selecting previously unselected package base-passwd.
(Reading database ... 0 files and directories currently installed.)
Preparing to unpack .../base-passwd_3.5.44_arm64.deb ...
/var/lib/dpkg/tmp.ci/preinst: 6: /var/lib/dpkg/tmp.ci/preinst: cannot create /etc/passwd: Permission denied
dpkg: error processing archive /var/cache/apt/archives/base-passwd_3.5.44_arm64.deb (--install):
 new base-passwd package pre-installation script subprocess returned error exit status 2
Errors were encountered while processing:
 /var/cache/apt/archives/base-passwd_3.5.44_arm64.deb

How can this error be resolved?

ラベル(2)
0 件の賞賛
返信
1 返信

2,754件の閲覧回数
Pavel
NXP Employee
NXP Employee

Your command sequence is correct.

Perhaps LSDK 1906 was not fully installed.

Use the following command sequence for LSDK 1906 installing under Ubuntu 8.04:

LSDK-1906 User Guide recommends the following command sequence for LSDK and Flex-build using:

1 .sudo apt-get install git

  1. tar xvzf flexbuild_lsdk1906.tgz
  2. source setup.env
  3. flex-builder -i mkrfs -a arm64
  4. flex-builder -c linux -a arm64

6 .flex-builder -i mklinux -a arm64 // .itb file

  1. flex-builder -i mkfw -m ls1046ardb -b sd // .img file is result of this command

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信