ethtool with eth1 does not work properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ethtool with eth1 does not work properly

2,370件の閲覧回数
Peter205652
Contributor I

Hi for all !!!

If DPSW is set in lx2160a NPU, ethtool with eth1 does not work properly. 

Please see the below for details .

jungyong_0-1663633249210.pngjungyong_0-1663633249210.png

In this case, how can i get the eth link and speed information?

Best regards

Peter.

0 件の賞賛
返信
3 返答(返信)

2,349件の閲覧回数
Peter205652
Contributor I

Hi yipingwang

Add an additional information :

Peter205652_0-1663755696272.pngPeter205652_0-1663755696272.png

Link detection and speed information did not change when the ethernet cable was disconnected from eth3 after the ethernet cable was connected to the eth3 port.

Please tell me why the ethernet information is not updated.

And In this case, how can i get the eth link and speed information?

Best regards

Peter.

0 件の賞賛
返信

2,326件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Which version LSDK are you using? And What's about the MC version?

0 件の賞賛
返信

2,354件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

 

Would you please provide more detailed information?

How did you set DPSW?

Please run "ls-listni" command on the target board to show which dpmac eth1 connects to.

Please connect Ethernet cable to eth1 port to check the link status with ethtool.

0 件の賞賛
返信