eTSEC1 in MII and eTsec3 in RGMII mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTSEC1 in MII and eTsec3 in RGMII mode

1,207件の閲覧回数
senoghte
Contributor II

Hi

According to this answer we decided to use eTSEC1 in MII and eTsec3 in RGMII mode but connect both L1VDD and LVDD to 2.5v and manage possible MII problems with timing barriers of course another side of this MII interace is supporting 2.5v.

But we have another problem with some sentences in AN4878 table 31 that "When eTSEC 1 or eTSEC 2 are configured as MII mode some of the MII 1 and MII 2 signals are muxed with eTSEC3 signals. In the RCW configuration eTSEC 3 must be selected as MII" .

AN4878.jpg

does it mean that RCW[EC3] can not be set 000 when we use eTSEC1 in MII? It should be said that MII optional pins not used in our design.

1021RM.jpg

Refer to table 4-14 of LS1021RM we want to set RCW[EC1]=011(MII) and RCW[EC3]=000(RGMII). this doesn't cause any conflict in register settings. May we assume it is possible?

Best Regards

Noghteh

ラベル(1)
0 件の賞賛
返信
1 返信

1,185件の閲覧回数
ufedor
NXP Employee
NXP Employee

EC3 must be 011 for MII support.

0 件の賞賛
返信