dpaa2_net: dpni disable failed (-110) DPAA2, DPDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dpaa2_net: dpni disable failed (-110) DPAA2, DPDK

1,751 Views
nic30
Contributor I

Hello,

I am using DPDK on LS2088ardb board.

I have allocated 1 DPNI and connected it to 1 DPMAC.1 (SPF+).

When I start DPDK testpmd application it works and can be closed only if incomming trafic is ~100 pkt/s.

If I send packets on wirespeed from another PC testpmd application can not be closed (even after traffic generator is stopped)

There is only one error:

Shutting down port 0...
Stopping ports...
dpaa2_net: dpni disable failed (-110)
dpaa2_net: Failure (ret -110) in disabling dpni 0 dev
Done
Closing ports...
dpaa2_net: Failure cleaning dpni device: err=-110
Done

If I run testpmd application it can not receive any packets.

Output from /dev/fsl_mc_console

[E:36f3b2a5ec, ifp_mng_cmd_enqueue:1708, CTLU]  Busy: No available Management command descriptor
[E:36f43fbafc, ifp_mng_cmd_enqueue:1708, CTLU]  Busy: No available Management command descriptor
[E:36f4cccaf0, ifp_mng_cmd_enqueue:1708, CTLU]  Busy: No available Management command descriptor

....

[E:36f9c18a2e, qbman_rec_isr:354, QBMAN]  QBMAN recoverable event 0x20040000
[E:36fb871426, qbman_rec_isr:387, QBMAN]  [FQ#7]: 12036

...

What does error -110 means? Is there any document about  /dev/fsl_mc_console ?

Labels (1)
0 Kudos
Reply
1 Reply

1,572 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello nic nic,

This is a known issue in our internal system, the development team is working on it now.

When killing the application while the traffic is running.

Application kill with print:

dpaa2_net: dpni disable failed (-110)
dpaa2_net: Failure (ret -110) in disabling dpni 2 dev
dpaa2_net: Failure cleaning dpni device: err=-110

 

After this - it is not possible to use the system for dpdk without re-starting the board.

Will fix this issue in the coming release.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply