can nand controller ECC has the ability to correct bit-flip in OOB area?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can nand controller ECC has the ability to correct bit-flip in OOB area?

2,499 次查看
luckyluo
Contributor II

Dear NXP,

I am using LS1088A in my product, I am sure that the nand controller ECC can fix the bit-flip in data area, but can nand controller ECC has the ability to correct bit-flip in OOB area? e.g if there is one bit-flip in OOB ecc position, this means the ecc content in OOB is wrong in one bit, so what will ECC do? can it detect this bit-flip and fix it?

Thanks a lot

Lucky Luo

标记 (1)
2 回复数

2,363 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Lucky Luo ,

The IFC computes the ECC only for the main region data (as the ECC is not computed for the spare region).

The decoder detects and corrects 4/8 bits of error on the main region data and the corresponding ECC bytes stored.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,363 次查看
luckyluo
Contributor II

So both main region data and the corresponding ECC bytes stored in OOB are ecc-protected, that's good for me.

thank you so much for your explanation.

0 项奖励
回复