can I deploy customized bootpartition, rootfs etc. using flex-installer?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can I deploy customized bootpartition, rootfs etc. using flex-installer?

1,882件の閲覧回数
Taeyoon
Contributor I

hi,

I have bootpartition, composite firmware, rootfs(ls-image-main.xxx.tar.gz) files customized with yocto build.

I confuse whether flex-installer command is used only when deploying default ones or also used for deploying customized ones. 

for example, if I have updated version(with customized kernel) ls-image-main-lx2160ardb-rev2.tar.gz in ~/yocto-sdk/build_lx2160ardb-rev2/tmp/deploy/images/lx2160ardb-rev2 directory, and run the command that $flex-installer -r ls-image-main-lx2160ardb-rev2.tar.gz -d /dev/sdx, then is updated rootfs in my host deployed to the SDcard connected to host?

 

thanks,

0 件の賞賛
返信
3 返答(返信)

1,862件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, flex-installer command can be used to deploy customized rootfs filesystem.

0 件の賞賛
返信

1,853件の閲覧回数
Taeyoon
Contributor I

so, I need to run flex-installer with working directory to be the directory that has customized rootfs file. right?

thanks

0 件の賞賛
返信

1,844件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes.

0 件の賞賛
返信