Yocto build vpp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build vpp

1,457件の閲覧回数
Blue_Sky1
Contributor II

Hi,

I refer to section 8.3.4.2 of the LLDP_6.1.55_2.2.0 documentation for the build vpp,used command:bitbake vpp,a very large number of rpm packages related to vpp have been generated in the following folder。

1、is this normal?Because in lsdk21.08, vpp will only generate 9 relevant deb package files.

2、How do I install vpp?

/root/yocto/build_lx2160ardb-rev2/tmp/work/aarch64-fsl-linux/vpp/2302-r0/deploy-rpms/aarch64

stupid_0-1722246315024.png

 

0 件の賞賛
返信
2 返答(返信)

1,434件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes  it is normal because is the dependencies of yocto and your apps. if you are in yocto, you have to build the whole package once it added to it.

regards

0 件の賞賛
返信

1,415件の閲覧回数
Blue_Sky1
Contributor II
Hi,Bio_TICFSL

Yes,i build vpp in yocto system,and i just run this command:bitbake vpp.

How do I take the compiled vpp and install it on the lx2160?

Thanks
0 件の賞賛
返信