Yocto Image BLUEBOX 3.0 Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Image BLUEBOX 3.0 Error

1,927 Views
AnanyaJamwal
Contributor I

Hello,
We are getting the following error after following the given documentation from NXP while generating Yocto Image for LX2160ARDB-REV2 for Bluebox 3.0 .

(We are using the documentation under NDA)
Command:
user@1234:/Layerscape/build_lx2160ardb-rev2$ bitbake ls-image-lite
ERROR:Nothing PROVIDES 'ls-image-lite'

We can see the .bb file at location '/Layerscape/sources/meta-nxp-desktop/recipes-fsl/images/ls-image-lite.bb'
Could we get some help to resolve this??

0 Kudos
Reply
2 Replies

1,785 Views
laodzu
Contributor IV

So I am running into the same problem now, with public documentation:

https://www.nxp.com/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf

Following the instructions from chapter 4.5 leads to this problem.  I see why this is the case, i.e. the mentioned "meta-nxp-desktop" layer is not enabled by default.  Instead, the "setup-env" script suggests building "fsl-image-networking" or "fsl-image-networking-full".

So I manually enabled the layer and bitbake starts running, but fails with this error:

ERROR: ParseError at /media/dzu/hd01-xfs/nxp/yocto-sdk-6.1.22-2.0.0/sources/meta-nxp-desktop/recipes-graphics/libgpuperfcnt/libgpuperfcnt_6.4.11.p1.2.1d.bb:8: Could not inherit file classes/fsl-eula-unpack2.bbclass
ERROR: Parsing halted due to errors, see error messages above

So I believe there are multiple problems here that need fixing by NXP, correct?

0 Kudos
Reply

1,901 Views
Oswalag
NXP TechSupport
NXP TechSupport

If you are using documentation under NDA please open a new technical case to review it.

0 Kudos
Reply