Which OpenWrt version or tag should I used on LS1012AFRWY?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which OpenWrt version or tag should I used on LS1012AFRWY?

Jump to solution
2,831 Views
paul7
Contributor II

Hi,

For now, I need to make decision for code-base select for LS1012AFRWY-base board.

Which OpenWrt version or tag below should I better used on LS1012AFRWY for development? Or you have better version suggest?

1. github.lede-project/openwrt-19.07

2. OpenWrt-19.04

BR,

Paul

0 Kudos
Reply
1 Solution
2,744 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Paul Young,

Currently the latest OpenWrt release from NXP is still OpenWrt-19.04, so I suggest you use OpenWrt-19.04.

A new version OpenWrt will be released in June of this year.

Thanks,

Yiping

View solution in original post

0 Kudos
Reply
3 Replies
2,745 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Paul Young,

Currently the latest OpenWrt release from NXP is still OpenWrt-19.04, so I suggest you use OpenWrt-19.04.

A new version OpenWrt will be released in June of this year.

Thanks,

Yiping

0 Kudos
Reply
2,744 Views
paul7
Contributor II

Hi Yiping,

OK, Got it.

But one problem I encounter is "crng init done" very late in booting on OpenWrt-19.04 snapshot. and OpenWrt-19.07 is no problem for this. Pls help to check and solve this issue on your official release. Thanks in advance.

BusyBox v1.30.1 () built-in shell (ash)

_______ ________ __
| |.-----.-----.-----.| | | |.----.| |_
| - || _ | -__| || | | || _|| _|
|_______|| __|_____|__|__||________||__| |____|
|__| W I R E L E S S F R E E D O M
-----------------------------------------------------
OpenWrt SNAPSHOT, r9781-e0a1b878cd
-----------------------------------------------------
=== WARNING! =====================================
There is no root password defined on this device!
Use the "passwd" command to set up a new password
in order to prevent unauthorized SSH logins.
--------------------------------------------------
root@OpenWrt:/# dmesg | grep crng
[ 0.000000] random: get_random_bytes called from start_kernel+0x80/0x420 with crng_init=0
root@OpenWrt:/# [ 258.865723] random: crng init done

BR

Paul

0 Kudos
Reply
2,744 Views
yipingwang
NXP TechSupport
NXP TechSupport

I will report this issue to OpenWrt development team.

0 Kudos
Reply