Where to make uboot and kernel changes to enable ecc_fix_en?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to make uboot and kernel changes to enable ecc_fix_en?

2,627 Views
tracysmith
Contributor IV

LS1043ARMv3 IFC has corrupted data disable reg 0x1080114 bit 30. If this bit is set then the corrupted data feature is disabled. When the corrupted data feature is enabled, the DDR controller will invert the generated ECC code for any beat of data which is known to have corrupted data. When a read to the corrupted data is later generated, the ERR_DETECT[CDE] error will be set if error reporting is enabled another field is DDR_SDRAM_CFG_3 1080260. ecc_fix_en is bit 1 and ecc_scrub_int is bit 4-7.  NXP has never enable this feature in the development boards because of the potential performance impact on memory. But I need to do periodic scrubbing and ECC error correction and will need to enable this feature of the IFC.

1) Where do I modify the code and what code changes are needed in the Linux kernel and uboot to enable ecc_fix_en and ecc_scrub_int?

2) For example, I see the following ddr_cfg_regs_1600.  Anything similar for the kernel and uboot source for the ls1043 ecc supported platforms?

3) I don't see this code in the fsl lsdk source available for download, will the code below be in the next release of the lsdk?

4) Is this from the most recent lsdk changes for the uboot ddr?

 https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/board/freescale/ls1043ardb...

 

#ifndef CONFIG_SYS_DDR_RAW_TIMING

fsl_ddr_cfg_regs_t ddr_cfg_regs_1600 = {

        .cs[0].bnds = 0x0000007F,

        .cs[1].bnds = 0,

        .cs[2].bnds = 0,

        .cs[3].bnds = 0,

        .cs[0].config = 0x80040322,

        .cs[0].config_2 = 0,

        .cs[1].config = 0,

        .cs[1].config_2 = 0,

        .cs[2].config = 0,

        .cs[3].config = 0,

        .timing_cfg_3 = 0x010C1000,

        .timing_cfg_0 = 0x91550018,

        .timing_cfg_1 = 0xBBB48C42,

        .timing_cfg_2 = 0x0048C111,

        .ddr_sdram_cfg = 0xC50C0008,

        .ddr_sdram_cfg_2 = 0x00401100,

        .ddr_sdram_cfg_3 = 0,

        .ddr_sdram_mode = 0x03010210,

        .ddr_sdram_mode_2 = 0,

        .ddr_sdram_mode_3 = 0x00010210,

        .ddr_sdram_mode_4 = 0,

        .ddr_sdram_mode_5 = 0x00010210,

        .ddr_sdram_mode_6 = 0,

        .ddr_sdram_mode_7 = 0x00010210,

        .ddr_sdram_mode_8 = 0,

        .ddr_sdram_mode_9 = 0x00000500,

        .ddr_sdram_mode_10 = 0x04000000,

        .ddr_sdram_mode_11 = 0x00000400,

        .ddr_sdram_mode_12 = 0x04000000,

        .ddr_sdram_mode_13 = 0x00000400,

        .ddr_sdram_mode_14 = 0x04000000,

        .ddr_sdram_mode_15 = 0x00000400,

        .ddr_sdram_mode_16 = 0x04000000,

        .ddr_sdram_interval = 0x18600618,

        .ddr_data_init = 0xDEADBEEF,

        .ddr_sdram_clk_cntl = 0x03000000,

        .ddr_init_addr = 0,

        .ddr_init_ext_addr = 0,

        .timing_cfg_4 = 0x00000002,

        .timing_cfg_5 = 0x03401400,

        .timing_cfg_6 = 0,

        .timing_cfg_7 = 0x13300000,

        .timing_cfg_8 = 0x02115600,

        .timing_cfg_9 = 0,

        .ddr_zq_cntl = 0x8A090705,

        .ddr_wrlvl_cntl = 0x8675F607,

        .ddr_wrlvl_cntl_2 = 0x07090800,

        .ddr_wrlvl_cntl_3 = 0,

        .ddr_sr_cntr = 0,

        .ddr_sdram_rcw_1 = 0,

        .ddr_sdram_rcw_2 = 0,

        .ddr_cdr1 = 0x80040000,

        .ddr_cdr2 = 0x0000A181,

        .dq_map_0 = 0,

        .dq_map_1 = 0,

        .dq_map_2 = 0,

        .dq_map_3 = 0,

        .debug[28] = 0x00700046,

 

};

Labels (2)
0 Kudos
Reply
2 Replies

2,351 Views
Pavel
NXP Employee
NXP Employee

Linux kernel does not change DDR configuration since Linux kernel works from DDR. Configuration of DDR is available in u-boot.

Configuration of the u-boot is available in the following folder in u-boot source: /include/configs/.

Look at the ls1043aqds.h and ls1043ardb.h files. These file are u-boot configuration file from SDK 2.0-1703.

Find the "#define CONFIG_DDR_ECC" in the ls1043aqds.h.

Use this define if your board uses DDR ECC.

 

If your board uses DIMM, the LS1043a reads DDR configuration from DIMM SPD.

Use the LS1043AQDS as example for DIMM using.

 

If your board does not use DIMM, use as example DDR configuration for the B4860qds board.

Find the "              .edc_config = 2,   /* ECC */" and "                 .ec_sdram_width = 8" in the b4860qds_ddr.c file.

See also attached fsl_ddr_dimm_params.h and the following page about ECC setting:

http://www.simmtester.com/page/news/showpubnews.asp?num=184

Find the "Module Memory Bus Width"

 

See also the ddr4_dimm_params.c from u-boot.

Find the following code:

                pdimm->primary_sdram_width = 1 << (3 + (spd->bus_width & 0x7));

                if ((spd->bus_width >> 3) & 0x3)

                               pdimm->ec_sdram_width = 8;

                else

                               pdimm->ec_sdram_width = 0;

                pdimm->data_width = pdimm->primary_sdram_width

                                                 + pdimm->ec_sdram_width;


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,351 Views
tracysmith
Contributor IV

The board does not use DIMM.

Can a driver be written from Linux to manage the ECC to enable the fix en init bit and to gather ECC statistics such as the number of errors corrected etc?

How would such a driver be designed? Is there an ECC interrupt that gets triggered each time there is an ECC error and/or correction?

0 Kudos
Reply