What is the best and worst case interrupt latency on the LS1043A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the best and worst case interrupt latency on the LS1043A?

1,858 Views
pro-supportengi
NXP Employee
NXP Employee

What is the best and worst case latency for interrupts on the LS1043A?  Latency between the occurrence of the interrupt and the start of the ISR.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,559 Views
lunminliang
NXP Employee
NXP Employee

Hello,

There is some description about the timings of interrupt signaling in the GIC-400 with physical interrupts, in GIC-400 RM.

This is an example, take SPIs and two level-sensitive N and M interrupts, the former with higher priority as example:

pastedImage_0.png

In Figure B-1, the latency at the physical interface is tph = 15 clock cycles.

The Distributor takes several cycles to calculate the highest priority pending interrupt. If an interrupt becomes pending while the calculation is in progress, it only affects the results of the next calculation. This means that the interrupt latency might vary. Therefore, while tph is typically 12 cycles, it might often be between 10 and 20 cycles.

The timings in Figure B-1 are for illustration only. They are typical values that are not guaranteed and must not be relied upon.

Regards

Lunmin

0 Kudos
Reply