HiLS1021A: Rev 2 : Can confirm the JTAG connector for Dstream is J12?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HiLS1021A: Rev 2 : Can confirm the JTAG connector for Dstream is J12?

Jump to solution
1,279 Views
shrikant_bobade
Contributor III

Hi,

I want to use Dstream DSTREAM – ARM Developer  for debugging along with LS1021A rev:2.0, I am using a 10 pin JTAG connector for connection at J12 connector. Is it correct connector ?

In Dstream case K20 JTAG  connector should not be used ?

Any pointers or references will be a great help!

Thanks

Shrikant

Labels (1)
Tags (1)
1 Solution
1,131 Views
ufedor
NXP Employee
NXP Employee

Is your request about the TWR-LS1021A board?

If "yes", then J12 has to be used for the debugger connection.

View solution in original post

4 Replies
1,131 Views
ufedor
NXP Employee
NXP Employee

Which NXP board is in question?

Please note that we do not support third-party tools.

1,131 Views
shrikant_bobade
Contributor III

Hi,

Board in question:  Layerscape 1021A rev 2.0: QorIQ LS1021A Dual-Core Communications Processor wi|NXP

Thanks for an update.

Thanks

Shrikant

0 Kudos
1,132 Views
ufedor
NXP Employee
NXP Employee

Is your request about the TWR-LS1021A board?

If "yes", then J12 has to be used for the debugger connection.

1,131 Views
shrikant_bobade
Contributor III

yes, TWR-LS1021A board, Thanks for confirming the J12 JTAG connector.

Thanks

Shrikant

0 Kudos