We try to boot up my platform LS1046, but it is can not boot.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We try to boot up my platform LS1046, but it is can not boot.

1,885件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team.

My platform is LS1046ardb.

We try to boot up my platform, but it is can not boot.

The error message:

NOTICE: UDIMM SQR-SD4I16G2K6SNCB

NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC off, CS0+CS1
NOTICE: BL2: v1.5(release):LSDK-20.12
NOTICE: BL2: Built : 10:29:16, Aug 16 2021
ERROR: BL2: Failed to load image (-2)
Authentication failure

The message is read my ddr (16 GB DDR4, 64-bit, CL=15, ECC off, CS0+CS1).

But Error is stop in BL2.

 

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

1,864件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please use CodeWarrior QCVS DDR Tool to validate the DDR controller settings.

0 件の賞賛
返信

1,819件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP @ufedor 

My board used the SO-DIMM DDR, do you have any advise about the different SO-DIMM DDR.

We need to modify ddr parameter for many different SO-DIMM DDR, right?

 

 

 

0 件の賞賛
返信

1,815件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try the latest LSDK 21.08.

If the issue still persists then it will be more convenient to open a Technical Case at:

https://support.nxp.com/

0 件の賞賛
返信

1,740件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

We need to focus the 20.12 LSDK .

Please provide the solution for LSDK 20.12

0 件の賞賛
返信

1,731件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please confirm that you have used CodeWarrior QCVS DDR Tool to validate the DDR controller settings.

0 件の賞賛
返信