We try to boot up my platform LS1046, but it is can not boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We try to boot up my platform LS1046, but it is can not boot.

1,886 Views
charleshuang
Senior Contributor II

Hi NXP Team.

My platform is LS1046ardb.

We try to boot up my platform, but it is can not boot.

The error message:

NOTICE: UDIMM SQR-SD4I16G2K6SNCB

NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC off, CS0+CS1
NOTICE: BL2: v1.5(release):LSDK-20.12
NOTICE: BL2: Built : 10:29:16, Aug 16 2021
ERROR: BL2: Failed to load image (-2)
Authentication failure

The message is read my ddr (16 GB DDR4, 64-bit, CL=15, ECC off, CS0+CS1).

But Error is stop in BL2.

 

Labels (2)
0 Kudos
Reply
5 Replies

1,865 Views
ufedor
NXP Employee
NXP Employee

Please use CodeWarrior QCVS DDR Tool to validate the DDR controller settings.

0 Kudos
Reply

1,820 Views
charleshuang
Senior Contributor II

Hi NXP @ufedor 

My board used the SO-DIMM DDR, do you have any advise about the different SO-DIMM DDR.

We need to modify ddr parameter for many different SO-DIMM DDR, right?

 

 

 

0 Kudos
Reply

1,816 Views
ufedor
NXP Employee
NXP Employee

Please try the latest LSDK 21.08.

If the issue still persists then it will be more convenient to open a Technical Case at:

https://support.nxp.com/

0 Kudos
Reply

1,741 Views
charleshuang
Senior Contributor II

Hi NXP Team

We need to focus the 20.12 LSDK .

Please provide the solution for LSDK 20.12

0 Kudos
Reply

1,732 Views
ufedor
NXP Employee
NXP Employee

Please confirm that you have used CodeWarrior QCVS DDR Tool to validate the DDR controller settings.

0 Kudos
Reply