VI display issue in LSDK Ubuntu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VI display issue in LSDK Ubuntu

1,790 Views
zcchai
Contributor I

Hello, Nxp community,

 I have tried both LSDK 18.09 and 18.12 on ls1012afrwy board. I could boot the Ubuntu and log in by either UART or SSH.

However, I couldn't edit the configure file with VI editor. Whenever I opened a file with VI, VI couldn't show the existing text, and moving the cursor (arrow keys) will end up printing wired character "@k" on the screen instead of scrolling. 

Does anyone have the same issue?

pastedImage_1.png

Thanks

0 Kudos
Reply
2 Replies

1,712 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Zhenchuan Chai,

I can reproduce your problem with Ubuntu 18.04.1 LTS rootfs built from LSDK 1812 release.

Please use vi command provided in busybox, it works normally, please use "busybox vi <your file>".


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,712 Views
zcchai
Contributor I

Hi Yiping,

Great, it works well.

Thanks for help

Zhenchuan

0 Kudos
Reply