Use L2 cache as SRAM on LS1012

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use L2 cache as SRAM on LS1012

847 Views
jordanrh
Contributor II

Is it possible to use the L2 cache as general purpose SRAM on LS1012 (before the cache is turned on)?

Tags (1)
0 Kudos
Reply
1 Reply

775 Views
Pavel
NXP Employee
NXP Employee

It is not possible. Use 128KBytes OCRAM of the LS1012a as SRAM.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply