Use L2 cache as SRAM on LS1012

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use L2 cache as SRAM on LS1012

1,303件の閲覧回数
jordanrh
Contributor II

Is it possible to use the L2 cache as general purpose SRAM on LS1012 (before the cache is turned on)?

タグ(1)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
Pavel
NXP Employee
NXP Employee

It is not possible. Use 128KBytes OCRAM of the LS1012a as SRAM.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信