Unresponsive netopeer-cli

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unresponsive netopeer-cli

1,872件の閲覧回数
sameer_chouksey
Contributor II

Hello all,

I am trying to connect netopeer client to a netopeer server. The server is running in the NXP, LS1028ARDB device. I am running the client in an Ubuntu machine.

When I try to connect the client with the server see following response on the server side:

netopeer-server[2044]: Adding new event (5)
netopeer-server[2044]: Created session 1 for user 'root' (UID 0) (recovery)
netopeer-server[2044]: New server session for 'root' with ID 1

Below is the response that I get on the client side.

netopeer-cli
netconf> verbose
Verbose level set to VERBOSE
netconf> connect --port 830 --login root 169.254.67.231
libnetconf VERBOSE: Publickey athentication
libnetconf VERBOSE: No key pair specified.
libnetconf VERBOSE: Password authentication (host 169.254.67.231, user root)
[email protected] password:

After this the terminal doesn't give the control back (no netconf> ). not able to issue any command after this.

Please check and help me know what I am missing. I am also adding complete logs from the server side in a file, please check.

Thanks,
Sameer

0 件の賞賛
返信
1 返信

1,757件の閲覧回数
bpe
NXP Employee
NXP Employee

Please update this thread with the versions of the software
running on the both host and the RDB. For the host, mention the
basic distribution name and the version of  netopeer
client; for LS1028A-RDB, the release of the LSDK or OpenIL that
was used to build the boot binaries.

Thanks,

Platon

0 件の賞賛
返信