Uboot debugging in code warrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot debugging in code warrior

2,236 Views
rashmikj
Contributor III

I am trying to debug uboot using code warrior in LS1046ardb Kit. I followed the steps mentioned in CodeWarrior for ARMv8 Using in u.pdf.

It always stops at Break at address "0x100000d0" with no debug information available, or outside of program code.

When i fuse the corresponding fip_uboot.bin file in qspi flash , uboot comes up and i can see in uart logs.

0 Kudos
Reply
1 Reply

2,210 Views
Pavel
NXP Employee
NXP Employee

Do you use the AN4876 for u-boot debugging? See the following document:

https://www.nxp.com/docs/en/application-note/AN4876.pdf

0 Kudos
Reply