UDP performance issue with 1088ARDB-PB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UDP performance issue with 1088ARDB-PB

2,948件の閲覧回数
ashutoshharry
Contributor III

Hi @yipingwang

we have 2 1088ARDB-PB connected back-to-back like WAN to WAN connected with 10G interface as WAN interface 

and we are tesing 10G speed optical but below is max speed we can achive 

TCP we are geting up to 9Gbs that good

but for UDP we are not geting more then 2.3Gbs 

we are testing using ipef client/server as testing.

 

please help 

タグ(1)
0 件の賞賛
返信
5 返答(返信)

2,927件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

 For UDP iperf test, you need to specify bandwidth with option "-b".

Sever: iperf -s -u

Client: iperf -c 100.1.1.99 -P 10 -t 30 -u -b 10G

0 件の賞賛
返信

2,899件の閲覧回数
ashutoshharry
Contributor III

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 件の賞賛
返信

2,893件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please compile Linux Kernel with CONFIG_NETFILTER and CONFIG_CPU_FREQ disabled

0 件の賞賛
返信

2,921件の閲覧回数
ashutoshharry
Contributor III

Hi 

 

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 件の賞賛
返信

2,937件の閲覧回数
ashutoshharry
Contributor III

@yipingwang  any help ?

0 件の賞賛
返信