UDP performance issue with 1088ARDB-PB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UDP performance issue with 1088ARDB-PB

2,961 Views
ashutoshharry
Contributor III

Hi @yipingwang

we have 2 1088ARDB-PB connected back-to-back like WAN to WAN connected with 10G interface as WAN interface 

and we are tesing 10G speed optical but below is max speed we can achive 

TCP we are geting up to 9Gbs that good

but for UDP we are not geting more then 2.3Gbs 

we are testing using ipef client/server as testing.

 

please help 

Tags (1)
0 Kudos
Reply
5 Replies

2,940 Views
yipingwang
NXP TechSupport
NXP TechSupport

 For UDP iperf test, you need to specify bandwidth with option "-b".

Sever: iperf -s -u

Client: iperf -c 100.1.1.99 -P 10 -t 30 -u -b 10G

0 Kudos
Reply

2,912 Views
ashutoshharry
Contributor III

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 Kudos
Reply

2,906 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please compile Linux Kernel with CONFIG_NETFILTER and CONFIG_CPU_FREQ disabled

0 Kudos
Reply

2,934 Views
ashutoshharry
Contributor III

Hi 

 

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 Kudos
Reply

2,950 Views
ashutoshharry
Contributor III

@yipingwang  any help ?

0 Kudos
Reply