UDP performance issue with 1088ARDB-PB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UDP performance issue with 1088ARDB-PB

2,930 次查看
ashutoshharry
Contributor III

Hi @yipingwang

we have 2 1088ARDB-PB connected back-to-back like WAN to WAN connected with 10G interface as WAN interface 

and we are tesing 10G speed optical but below is max speed we can achive 

TCP we are geting up to 9Gbs that good

but for UDP we are not geting more then 2.3Gbs 

we are testing using ipef client/server as testing.

 

please help 

标记 (1)
0 项奖励
回复
5 回复数

2,909 次查看
yipingwang
NXP TechSupport
NXP TechSupport

 For UDP iperf test, you need to specify bandwidth with option "-b".

Sever: iperf -s -u

Client: iperf -c 100.1.1.99 -P 10 -t 30 -u -b 10G

0 项奖励
回复

2,881 次查看
ashutoshharry
Contributor III

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 项奖励
回复

2,875 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please compile Linux Kernel with CONFIG_NETFILTER and CONFIG_CPU_FREQ disabled

0 项奖励
回复

2,903 次查看
ashutoshharry
Contributor III

Hi 

 

yes we used same commands to test , but same result TCP max 6GBs and UDP max 2.3GBs

0 项奖励
回复

2,919 次查看
ashutoshharry
Contributor III

@yipingwang  any help ?

0 项奖励
回复