UART registar (UARTMISC) specifications for LX2160A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART registar (UARTMISC) specifications for LX2160A

3,129件の閲覧回数
shiota_kotaro
Contributor I

Hello.

Regarding the behavior of the UARTMISC register, I think there is a difference between the document description and the implementation.By setting 1, is it correct that "Interrupts occur when the interrupt mask is released"?

According to Section 29.6.1.10 of the QorIQ LX 2160 A Reference Manual, Rev. 1, 10/2021, with the following statement,it has been determined that "Interrupt Mask Settings" is 1.

The UARTIMSC register is the interrupt mask set/clear register. It is a read/write register.
On a read this register returns the current value of the mask on the relevant interrupt. On a write of 1 to the particular bit, it sets the corresponding mask of that interrupt. A write of 0 clears the corresponding mask. All the bits are cleared to 0 when reset.

When I checked the operation with the evaluation board, the reception interrupt occurs by setting 1.

Best regards.


0 件の賞賛
返信
3 返答(返信)

3,052件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Can you please provide the UART register dump before and after writing to the UARTIMSC register.

0 件の賞賛
返信

3,016件の閲覧回数
shiota_kotaro
Contributor I

The collected information is attached. (collected on TRACE 32)

0 件の賞賛
返信

2,992件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

When I checked the operation with the evaluation board, the reception interrupt occurs by setting 1.
--> According to the provided register dump, when you write to the UARTIMSC register (all interrupt mask set), no bit is set in UARTRIS. This means that you are not receiving any interrupts.

Please provide the steps to reproduce this issue on LX2160ARDB.

0 件の賞賛
返信