U-Boot 2015.01QorIQ-SDK-V1.7+gc297f5b (Dec 20 2015 - 13:08:26)
I am able to successfully unprotect and copy (cp) to arbitrary memory spaces, but other commands like memory modify (mm) and memory write (mw) do not work. For example:
=> protect off 0x60300000 0x6031FFFF
Un-Protected 1 sectors
Sector Start Addresses:
...
601E0000 E RO 60200000 RO 60220000 E RO 60240000 E RO 60260000 E RO
60280000 E RO 602A0000 E RO 602C0000 E RO 602E0000 E RO 60300000 E
60320000 E RO 60340000 E RO 60360000 E RO 60380000 E RO 603A0000 E RO
...
=> md.b 0x60300000 10
60300000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
=> mm 0x60300000
60300000: ffffffff ? aa
60300004: ffffffff ? bb
60300008: ffffffff ? cc
6030000c: ffffffff ? dd
60300010: ffffffff ? ee
60300014: ffffffff ? .
=> md.b 0x60300000 10
60300000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
However, if I copy from another memory location it seems to work as expected:
=> cp.b 0 0x60300000 10
Copy to Flash... done
=> md.b 0x60300000 10
60300000: 00 00 01 10 00 c0 1e d5 01 10 3e d5 82 00 80 d2 ..........>.....
After erasing the sector and removing write permissions (e.g. protect on all) I get the following error when trying to copy, so it does not appear to be a problem with protections.
=> protect on all
Protect Flash Bank # 1
=> flinfo
Sector Start Addresses:
...
601E0000 E RO 60200000 RO 60220000 E RO 60240000 E RO 60260000 E RO
60280000 E RO 602A0000 E RO 602C0000 E RO 602E0000 E RO 60300000 E RO
60320000 E RO 60340000 E RO 60360000 E RO 60380000 E RO 603A0000 E RO
...
=> cp.b 0 0x60300000 10
Copy to Flash... Can't write to protected Flash sectors
Even an external JTAG programmer fails to write to memory with a halted CPU (verification failure).
 
					
				
		
 marius_grigoras
		
			marius_grigoras
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
This is normal behavior, because mm command is used only to modify a volatile memory as RAM. For modifying the flash content memory you need to use the cp command.
The same is for using the tools - cannot write/modify the flash content using memory view, but instead you need to use Flash Programmer.
Thank you,
Marius
Described behaviour is by design.
Only "cp" is capable to write to flash - refer to the U-Boot Quick Reference, 4.10 CP:
http://cache.freescale.com/files/32bit/doc/quick_ref_guide/MEDIA5200UBPG/MEDIA5200UBPG.pdf
I see. I was able to contrive a workaround to solve my problem. Thank you for the swift responses!