Trust Zone required for DDR Memory access?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trust Zone required for DDR Memory access?

Jump to solution
2,351 Views
userland
Contributor II

Hi

I've been looking into the DDR driver on BL2 and noticed that Trust Zone sets up access to the memory areas, same when looking into the CW scripts. Is Trust Zone required to be initialized for the DDR memory to be accessible?

I know that MMU is not required for it but is it the same with TZ?

 

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,293 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, LSDK boot up the device with TF-A (Trusted Firmware for ARM). That required isolate resource, including DDR memory, etc.

If customer don't use OPTEE or Trust Zone, they should able to do without DDR setup. (e.g. taking the PPA approach(i.e. Non TF-A). However, PPA example are not available with LX2160A) More explanation on TrustZone/OPTEE are in the LSDK User Guide.

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-9280C0B6-CE8D-411D-9...

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-61AC454A-C6DD-46AD-8...

View solution in original post

0 Kudos
Reply
1 Reply
2,294 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, LSDK boot up the device with TF-A (Trusted Firmware for ARM). That required isolate resource, including DDR memory, etc.

If customer don't use OPTEE or Trust Zone, they should able to do without DDR setup. (e.g. taking the PPA approach(i.e. Non TF-A). However, PPA example are not available with LX2160A) More explanation on TrustZone/OPTEE are in the LSDK User Guide.

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-9280C0B6-CE8D-411D-9...

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-61AC454A-C6DD-46AD-8...

0 Kudos
Reply