To implement Read-While-Write (RWW) functionality on the LS1043A SoC ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To implement Read-While-Write (RWW) functionality on the LS1043A SoC ?

1,755 Views
lgx
Contributor I

I need to implement Read-While-Write (RWW) functionality on the LS1043A SoC.

cs0 is the boot sNOR, works on XIP mode, cs1 is the data sNOR.

I find the similar implementation on MCU serial 

https://www.nxp.com.cn/docs/en/application-note/AN12564.pdf

 

Do we have the demo logic to implement RWW on ls1043a ?

Tags (1)
0 Kudos
Reply
3 Replies

1,668 Views
yipingwang
NXP TechSupport
NXP TechSupport

I contacted the AE team, please refer to the following feedback from them.

In theory, RWW is supported, but we don't have such demo/case.

It becomes harder if it was used at boot stage because the qspi driver was initialized quite late.
On RT10xx board, there is uboot or other bootloader, so it is easier to implement it.

I am asking R&D team for help, will inform you if got any progress, but no guarantee to get the demo.

0 Kudos
Reply

1,665 Views
lgx
Contributor I
Thanks.
On ls1043a, it also run arm-trusted-firmware (atf) and then uboot. I think qspi could be configured during bl2 stage.
0 Kudos
Reply

1,648 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes, that means you need to implement the RWW in ATF stage. We don't have such demo for reference.

If you implement it in driver in kernel, then that would be easier. Please refer to arch/arm64/boot/dts/freescale/fsl-ls208xa-qds.dtsi:
See attached. It supports 2 flash chip at the same time. select the chip by property: reg=0 and reg=2.

0 Kudos
Reply