The available capacity of the LX2160ARDB_REV2 DDR4 is 2 GB less than the actual physical capacity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The available capacity of the LX2160ARDB_REV2 DDR4 is 2 GB less than the actual physical capacity

Jump to solution
2,083 Views
liushuangxin
Contributor III

Hello nxp,

we use 2160 as CPU,LSDK 20.4,linux 5.4.3. We used 8 pieces of ddr particles with a capacity of 1GB. After entering the system, we used the free command to query only about 5.7G, which is more than 2 G less than the actual. We queried NXP's official lx2160ardb_rev2 demo board and found that the 32G physical memory display is only 29.7G.
I would like to ask if this kind of imagination exists in the SDK, or if there are other configurations that can be configured.

Thank you. Hope to get your reply!

Tags (1)
0 Kudos
Reply
1 Solution
2,038 Views
yipingwang
NXP TechSupport
NXP TechSupport

The lost DDR can be divided into 2 parts.
1) DDR used by NXP specific software, firmware components
2) DDR used by various segments of kernel.

For the first part,
1) u-boot uses memory till it is used, but once kernel boots, u-boot is swapped out of memory.
2) 66 MB is used by TF-A
3) MC can use anywhere between 512M to 2G (it depends on u-boot comandline argument 'mcmemsize'). The parameter mcmemsize defines amount of system DDR to be used by the Management Complex. If this variable is not defined, the compile-time value 0x70000000 or 1.75GB will be the default. Normally, users do not need to set this variable because the default is acceptable.

TF-A+MC is about 1.8G

kernel reserved=(18620K kernel code, 2476K rwdata, 8844K rodata, 5888K init, 993K bss, 406712K reserved, 327680K cma-reserved) = 771213K=0.7G

MemTotal in /proc/meminfo is 14232028 kB, the lost memory is about 16-13.6=2.4G(TF-A+MC+kernel reserved)

root@TinyLinux:~# cat /proc/meminfo
MemTotal: 14232028 kB
MemFree: 13596760 kB
MemAvailable: 13478276 kB

View solution in original post

0 Kudos
Reply
3 Replies
2,039 Views
yipingwang
NXP TechSupport
NXP TechSupport

The lost DDR can be divided into 2 parts.
1) DDR used by NXP specific software, firmware components
2) DDR used by various segments of kernel.

For the first part,
1) u-boot uses memory till it is used, but once kernel boots, u-boot is swapped out of memory.
2) 66 MB is used by TF-A
3) MC can use anywhere between 512M to 2G (it depends on u-boot comandline argument 'mcmemsize'). The parameter mcmemsize defines amount of system DDR to be used by the Management Complex. If this variable is not defined, the compile-time value 0x70000000 or 1.75GB will be the default. Normally, users do not need to set this variable because the default is acceptable.

TF-A+MC is about 1.8G

kernel reserved=(18620K kernel code, 2476K rwdata, 8844K rodata, 5888K init, 993K bss, 406712K reserved, 327680K cma-reserved) = 771213K=0.7G

MemTotal in /proc/meminfo is 14232028 kB, the lost memory is about 16-13.6=2.4G(TF-A+MC+kernel reserved)

root@TinyLinux:~# cat /proc/meminfo
MemTotal: 14232028 kB
MemFree: 13596760 kB
MemAvailable: 13478276 kB

0 Kudos
Reply
2,017 Views
liushuangxin
Contributor III
Dear yiping,
Thank you for your reply, your answer is very helpful to me.
Best regrards
0 Kudos
Reply
2,079 Views
liushuangxin
Contributor III
 
0 Kudos
Reply