Testing kdump/kexec on ls2085ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Testing kdump/kexec on ls2085ardb

1,786件の閲覧回数
denyszagorui
Contributor I
ラベル(1)
0 件の賞賛
返信
1 返信

1,543件の閲覧回数
denyszagorui
Contributor I

Hello,

Particular question, how turn on PSCI cpu enable method? Using uBoot from Qoriq SDK 2.0 have this log:

U-Boot 2016.092.0+g2735535 (Mar 17 2017 - 22:45:15 +0200)

SoC: LS2085AE Rev1.0 (0x87010010)
Clock Configuration:
CPU0(A57):1800 MHz CPU1(A57):1800 MHz CPU2(A57):1800 MHz
CPU3(A57):1800 MHz CPU4(A57):1800 MHz CPU5(A57):1800 MHz
CPU6(A57):1800 MHz CPU7(A57):1800 MHz
Bus: 600 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 48303830 48480048 00000000 00000000
00000010: 00000000 00200000 00200000 00000000
00000020: 00c12980 00002580 00000000 00000000
00000030: 00000e0b 00000000 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 412a0000 00000000 00000000 00000000
Model: Freescale Layerscape 2080a RDB Board
Board: LS2085AE Rev1.0-RDB, Board Arch: V1, Board version: D, boot from vBank: 0
FPGA: v1.18
SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz
SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ASF1G72AZ-2G1A1
Detected UDIMM 18ASF1G72AZ-2G1A1
DP-DDR: Detected UDIMM 18ASF1G72AZ-2G1A1
19 GiB
DDR 15 GiB (DDR4, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 256B
DDR Chip-Select Interleaving Mode: CS0+CS1
DP-DDR 4 GiB (DDR4, 32-bit, CL=11, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
PSCI: PSCI does not exist.
Waking secondary cores to start from fff00000
All (8) cores are up.
Using SERDES1 Protocol: 42 (0x2a)
Using SERDES2 Protocol: 65 (0x41)
Flash: 128 MiB
NAND: 2048 MiB
MMC: FSL_SDHC: 0
EEPROM: Invalid ID (ff ff ff ff)
In: serial
Out: serial
Err: serial
Debug Server FW: Not a FIT image
SEC0: RNG instantiated
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net: PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 disabled
PCIe2: pcie@3600000 Root Complex: x1 gen1
PCIe3: pcie@3700000 Root Complex: no link
e1000: 68:05:ca:36:9b:0d
DPMAC1@xgmii, DPMAC2@xgmii
Warning: DPMAC2@xgmii (eth1) using random MAC address - 9e:9c:cf:1d:72:65
, DPMAC3@xgmii, DPMAC4@xgmii
Warning: DPMAC4@xgmii (eth3) using random MAC address - c6:c4:75:f4:50:9e
, DPMAC5@xgmii
Warning: DPMAC5@xgmii (eth4) using random MAC address - ce:cc:5c:8e:dc:92
, DPMAC6@xgmii
Warning: DPMAC6@xgmii (eth5) using random MAC address - 52:7d:51:5b:81:c7
, DPMAC7@xgmii, DPMAC8@xgmii
Warning: DPMAC8@xgmii (eth7) using random MAC address - 7a:74:bd:6e:dc:1b
, e1000#0 [PRIME]
Warning: e1000#0 MAC addresses don't match:
Address in SROM is 68:05:ca:36:9b:0d
Address in environment is 68:05:ca:2e:24:ee

Best regards,

Denys

0 件の賞賛
返信