Test suite for kernel & uboot release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Test suite for kernel & uboot release

3,394件の閲覧回数
tracysmith
Contributor IV

What does NXP use to validate SDK 2.0 kernel and u-boot releases for stability and regression?

 What are possible test suites available to test for stability?

Is NXP using LTP for regression testing, or for unit or functional testing?  LTP - Linux Test Project 

Is NXP using the Phoronix Test Suite for regression testing? Phoronix Test Suite - Linux Testing & Benchmarking Platform, Automated Testing, Open-Source Benchmar... 

ラベル(2)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,075件の閲覧回数
tracysmith
Contributor IV

I don't see any memory or ECC validation in the logs provided?  Are memory and ECC tests available as part of the LTP used and modified by NXP?

0 件の賞賛
返信

3,074件の閲覧回数
tracysmith
Contributor IV

NXP is using LTP to test the QorIQ LS1043 BSP. Requires and customer support contract to obtain the code. Testing being done in China.

0 件の賞賛
返信

3,074件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tracy Smith,

LTP is used in the regression test by the testing team. In fact, we have internal automation test Tool(LARS) to help the testing team to do function and performance test, which is totally developed by NXP.

Please refer to the following part of the test report.

functional/dpaa_ethernet/linux_dpaa_ethernet_bridging_iperf_par_tcp_1G_b2b.py log 7M 14SPass
functional/dpaa_ethernet/linux_dpaa_iperf_par_tcp_10G_b2b.py log 6M 27SPass
functional/dpaa_ethernet/linux_dpaa_iperf_par_tcp_1G_b2b.py log 9M 46SPass
functional/dpaa_ethernet/linux_dpaa_ipv6_floodping_10G_b2b.py log 5M 22SPass
functional/dpaa_ethernet/linux_dpaa_ipv6_floodping_1G_b2b.py log 5M 38SPass
functional/dpaa_ethernet/linux_dpaa_ipv6_iperf_par_tcp_10G_b2b.py log 6M 15SPass
functional/dpaa_ethernet/linux_dpaa_ipv6_iperf_par_tcp_1G_b2b.py log 9M 34SPass
functional/dpaa_ethernet/linux_dpaa_jumboframe_floodping_10G_b2b.py log 5M 17SPass
functional/dpaa_ethernet/linux_dpaa_jumboframe_floodping_1G_b2b.py log 5M 20SPass
functional/dpaa_ethernet/linux_dpaa_jumboframe_iperf_par_tcp_10G_b2b.py log 6M 41SPass
functional/dpaa_ethernet/linux_dpaa_jumboframe_iperf_par_tcp_1G_b2b.py log 6M 44SPass
functional/dpaa_ethernet/linux_dpaa_netperf_tcp_sendfile_10G_b2b.py log 6M 31SPass
functional/dpaa_ethernet/linux_dpaa_netperf_tcp_sendfile_1G_b2b.py log 6M 27SPass
functional/dpaa_ethernet/linux_dpaa_vlan_floodping_10G_b2b.py log 10M 42SPass
functional/dpaa_ethernet/linux_dpaa_vlan_floodping_1G_b2b.py log 7M 41SPass
functional/dpaa_ethernet/linux_dpaa_vlan_iperf_par_tcp_10G_b2b.py log 8M 26SPass
functional/dpaa_ethernet/linux_dpaa_vlan_iperf_par_tcp_1G_b2b.py log 8M 22SPass
functional/dpaa_ethernet/linux_dpaa_vlan_scp_10G_b2b.py log 6M 43SPass
functional/dpaa_ethernet/linux_dpaa_vlan_scp_1G_b2b.py log 7M 20SPass
functional/dpaa_fman/fman_debug.py log 2M 41SPass
functional/ethtool/linux_ethtool_offload_sg.py log 11M 49SPass
functional/ethtool/linux_ethtool_stat.py log 2M 17SPass

For LTP test code requirement, please create an internal service request to get it.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,570件の閲覧回数
ArifSharief
Contributor I

Please let me know how to create internal request for above mentioned LTP (LARS) for testing NXP i.MX8M plus kernel and uboot .

0 件の賞賛
返信