Technical documentation for the reference design version of ls1043aqds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technical documentation for the reference design version of ls1043aqds

2,012 Views
qzl1202
Contributor I

I am debugging a circuit board based on the ls1043a processor, using QSPI download and IFC bus. I encountered some problems during debugging. Can you provide the schematic diagram, reference manual, and other technical materials of the ls1043aqds development board?

0 Kudos
Reply
3 Replies

1,966 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For the LS1043AQDS reference design, I can provide you with the following resources:

1. The LS1043AQDS Reference Manual - This document contains detailed information about the architecture, bus protocols, memory map, and peripheral interfaces including the QSPI and IFC bus configurations you're working with.

2. Schematic Diagrams - These provide the circuit-level implementation details that would be helpful for debugging your board.

3. QorIQ LS1043A Reference Design Materials - These include the board design files, component datasheets, and implementation guidelines.

You can access these materials through the NXP website in the QorIQ processors documentation section. Specifically, look under the LS1043A product page where reference design materials are available for download.

If you have specific issues with the QSPI download or IFC bus implementation, I recommend also checking the LS1043A SoC Reference Manual which provides detailed register-level information for these interfaces.

Regards

0 Kudos
Reply

1,470 Views
qzl1202
Contributor I
Sorry, I couldn't find any information about the ls1043aqds development board on the NXP website. Can you provide a download link for these information
0 Kudos
Reply

1,894 Views
qzl1202
Contributor I
Sorry, I couldn't find any information about the ls1043aqds development board on the NXP website. Can you provide a download link for these information
0 Kudos
Reply