TFTP in binary mode? ls1021a-twr

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TFTP in binary mode? ls1021a-twr

跳至解决方案
4,561 次查看
datho
Contributor III


I'm currently using a ls1021a-twr rev 2 board, that has a tftp command (GNU inetutils 1.9.2). This tftp command doesn't have a way to specify a binary mode. When I tftp files from Linux it works just fine but I also want to tftp files from a Windows server. Without the binary mode for the tftp, a lot of the files I get from Windows become unusable.

Is there a way to update the tftp command to allow for binary mode? or is there another way to get files from a windows machine without corrupting them?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
4,140 次查看
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

在原帖中查看解决方案

0 项奖励
回复
1 回复
4,141 次查看
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

0 项奖励
回复