System keeps reboot due to UART RX pin left floating ls1021a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System keeps reboot due to UART RX pin left floating ls1021a

1,549 Views
jiye
Contributor V

Hi,

My system keeps reboot due to the UART RX keep sending nonsense characters during boot, in my circuit I left this pin as floating but I dont want to change the hardware layout as it will cost a lot. 

I still want to use RX for debugging and I dont want to disable to affect my debugging.

The driver is pl011

(1) Is there way to fix this in a software way? disable this driver at bootrom and re-enable them back 

I just want to find a way to disable the RX during bootrom then enable it back 

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,460 Views
ufedor
NXP Employee
NXP Employee

Which exactly "UART RX" is in question?

What does it mean: "The driver is pl011"?

What does it mean: "My system keeps reboot"?

Please provide detailed technical description of the problem including the following attachments:

1) the processor connection schematics as searchable PDF

2) digital scope traces showing behaviour of the processor's reset signals corresponding to the  QorIQ LS1021A Reference Manual, Figure 4-1. Power-on reset sequence

0 Kudos
Reply