Scarthgap Images Fail to Boot on Custom LS1012A Board via SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Scarthgap Images Fail to Boot on Custom LS1012A Board via SD Card

3,109 Views
Dhanyalakshmi
Contributor III

We are encountering a boot issue on our custom LS1012A-based board when using rootfs and boot-partition images generated from the Scarthgap branch, while booting from the SD card.

What Works:

  • On the FRWY-LS1012A evaluation board, both Mickledore and Scarthgap branch images (rootfs & boot-partition) boot successfully from the SD card.

  • On our custom board, images (rootfs & boot-partition) built from the Mickledore branch boot successfully from the SD card.

What Fails:

  • On our custom board, the system fails to boot when using the Scarthgap branch images (rootfs & boot-partition) from the SD card. The kernel appears to hang shortly after starting.

Hardware Differences (Custom Board vs. FRWY-LS1012A):

Our custom board is derived from the FRWY-LS1012A with the following minor hardware changes:

  • Audio input/output ports removed

  • M.2 Type-E NGFF slot removed

  • mikroBus Click headers removed

Other components and peripherals remain unchanged.

SDK Source:


Please let us know if the image build steps or SD card preparation process are needed for verification. We are happy to provide complete logs and reproduction steps.

0 Kudos
Reply
7 Replies

3,063 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download Scarthgap prebuilt Kernel image and dtb file from the following link.

https://support.nxp.com/s/case/500Tg00000KC1b9IAD/community-scarthgap-images-fail-to-boot-on-custom-...

Please refer to the following command to boot Kernel Image.

=>tftp 0xa0000000 Image

=>tftp 0xb0000000 fsl-ls1012a-frwy.dtb

=> booti 0xa0000000 - 0xb0000000

Please check whether you get the same error on your custom board.

If yes, please use mtest command to test DDR memory in u-boot.

0 Kudos
Reply

3,051 Views
Dhanyalakshmi
Contributor III

Thank You Yiping for the reply,

I tried with the dtb and image you have provided but SD card still did not boot properly. I have attached the logs for your reference. Please provide guidance why SDK built from scarthgap branch unable to boot from SD card. 

And how to resolve this issue.

Thank You

0 Kudos
Reply

3,006 Views
yipingwang
NXP TechSupport
NXP TechSupport

The system didn't stop at the same place, so I suspect there is problem with your DDR controller initialization.

What's the result to do DDR test with "mtest" command?

Did you find any error?

0 Kudos
Reply

2,997 Views
Dhanyalakshmi
Contributor III
Thank You Yiping for the reply,Here's the result of the command.

=> mtest
Testing 80000000 ... 9fffffff:
Pattern 0000000000000000 Writing...


it stuck here only for about 5 minutes. Is it normal?
0 Kudos
Reply

2,994 Views
yipingwang
NXP TechSupport
NXP TechSupport

It's abnormal, the DDR test program cannot run normally at all.

Please use QCVS DDRv tool to connect to your custom board to do optimization and validation.

0 Kudos
Reply

2,992 Views
Dhanyalakshmi
Contributor III
Can you guide me to perform optimization and validation using DDRv tool.

Also,I have a doubt if the same custom board able to boot SD card which has rootfs and boot-partition images built from mickledore and styhead branch then why not working for sacrthgap?
0 Kudos
Reply

2,952 Views
yipingwang
NXP TechSupport
NXP TechSupport

For QCVS DDRv tool usage, you could refer to the following document.

https://www.nxp.com.cn/docs/en/user-guide/QCVS_DDR_User_Guide.pdf

https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-B...

You could use "read from target" method to create a QCVS DDR project, then connect to your target board to do validation to get the optimized parameters.

After successful validation, please click Project->Generate Processor Expert Code to get the optimized DDR controller configuration parameters in file ddr_init1.c, and use it to modify ATF source code plat/nxp/soc-ls1012a/ls1012afrwy/ddr_init.c.

0 Kudos
Reply