SError interrupt due to LDAXRB instruction when disable cache on ls1046a RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SError interrupt due to LDAXRB instruction when disable cache on ls1046a RDB

2,183 Views
Tonyx
Contributor II

Hi Experts

My code runs in EL3 on ls1046a RDB in bare mental environment. Here are the focus code after start up.

Step 1: Disable data cache cache, the the sctlr_el3 is changed from 0x00c5183d to 0x00c51839

Step 2: Update a global variable.

Step 3: do {} while (atomic_flag_test_and_set(&gIRQpRrintmutex));

0000000080005a68: adrp x0, 0x8002e000 <__global_locale+120>
0000000080005a6c: add x0, x0, #0x1b8
0000000080005a70: mov w1, #0x1 // #1
0000000080005a74: ldaxrb w2, [x0]

SError interrupt happened in Step 3: when execute "ldaxrb w2, [x0]" as the resister value as below:

ESR_EL3: 0xbf000002

ELR_EL3: 0x0000000080005a74

If not disable cache as in the step 1, the code execute well.

 

FUNC_START __asm_disable_dcache
isb
mrs x0, sctlr_el3
bfi w0, wzr, #2, #1 // Disables data cache
msr sctlr_el3, x0
isb
ret

Tags (3)
0 Kudos
Reply
5 Replies

2,163 Views
Tonyx
Contributor II

Try disable I Cache, MMU and invalidate TLB, still not work.

sctlr_el1, sctlr_el2, sctlr_el3 is changed from 0x00c5183d to 0x00c50838

0 Kudos
Reply

2,135 Views
yipingwang
NXP TechSupport
NXP TechSupport
Have you tried to disable data cache before you declared the global variable. If yes, please share the results.
0 Kudos
Reply

2,132 Views
Tonyx
Contributor II

Not sure about "disable data cache before you declared the global variable".

Since "disable data cache" is at run time and "declared the global variable" is done in a location of a source code file....

0 Kudos
Reply

2,116 Views
yipingwang
NXP TechSupport
NXP TechSupport

Try to flush the data cache before you disable it.

0 Kudos
Reply

2,174 Views
Tonyx
Contributor II

May be need to flush the case and invalidate TLBs as in the u-boot code

flush_dcache_all();
__asm_invalidate_tlb_all();

0 Kudos
Reply