SERDES 3-taps equalization LX2160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SERDES 3-taps equalization LX2160

2,138 Views
FRO
Contributor I

Dear,

I would like to perform a 3-tap equalization on SERDES 1 of LX2160 (lanes 4 to 7).

I write into register LNmTECRO at address 0x1ea0c30 (lane 4) to address 0x1ea0f30 (lane 7) the parameters (pre, post and main cursor) but nothing change on the signal (seen with an oscilloscope).

Is there an other register to write in to activate equalization ?

Thank you ! 

0 Kudos
Reply
3 Replies

2,126 Views
FRO
Contributor I

1) SerDes 1 is 40G Ethernet

2) Lane 4, 5, 6 & 7, QCVS SerDes Validation Tool is not used (direct register programming by shell command)

3) Before modification, values are 0x20828700 (bit 32..0) (same value on all lanes)

After modification, values are 0x20828710 (EQ_AMP_RED set to 0.5)

What do you mean by "after exiting the test"? after a reboot? If it's the case, values are set to the same as before modification (0x20828700)

 

0 Kudos
Reply

2,116 Views
ufedor
NXP Employee
NXP Employee

Let's continue in the Technical Case #00361573

0 Kudos
Reply

2,130 Views
ufedor
NXP Employee
NXP Employee

1) Which SerDes1 protocol is configured?

2) How exactly lanes are tested? Is QCVS SerDes Validation Tool used?

3) What are values of LNmTECR0 before modification, after modification and after exiting the test?

0 Kudos
Reply