SEC RTA and secengine for LS1046

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEC RTA and secengine for LS1046

4,221件の閲覧回数
roger_davis
Contributor II

I would like to make use of the security engine in the LS1046 and am interested to find out if there are any source code samples or libraries for it.  I found a brochure that references SEC RTA Library that might be helpful but can't find any information on it and not sure if it would be helpful. 

I know that other NXP processors such as the S32K have reference source code designs for some of the security components like for the CSE interface, and would very much like to find if something like that is available for this LS1046 processor or similar processor with the same security engine.

0 件の賞賛
返信
5 返答(返信)

4,199件の閲覧回数
roger_davis
Contributor II

RTIC is interesting, but we intend on performing a secure boot and also to use the crypto engine for some other general purpose crypto operations. I found a brochure that mentions SEC RTA as if that might help to configure it, but have not found any details on it. This is the first crypto engine that we have encountered that did not have sample or library code to support the engine.

0 件の賞賛
返信

4,195件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Regards to crypto engine SEC RTA, it is documented in the LSDK user guide.

 

The RTA documentation is in

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/G

UID-AB2B4FFB-74A4-49DC-85C1-81EA026863C5.html#GUID-AB2B4FFB-74A4-49DC-85C1-8

1EA026863C5

#####

Runtime Assembler Library Reference

Last updated Dec 28, 2017

Use the Runtime Assembler Library to write SEC descriptors.

 

Runtime Assembler Library Reference

Use the Runtime Assembler Library to write SEC descriptors. This reference

describes the structure, concept, functionality, and high-level API.

The following section contains Writing Descriptors for NXP CAAM using RTA

Library. The guide is available in a downloadable ZIP package and in a PDF

format.

 

Click this link to view PDF output for this document.

 

Click this link to download the NXP CAAM using RTA Library ZIP package. To

open the NXP CAAM using RTA Library, download the ZIP package and extract

the files, as explained in the following steps.

Extract the files using any file archiver and compressor utility, for

example 7Zip.

After extracting, double-click the Start Here file to open the Reference

Manual in your default browser.

If you are working in a Linux environment, browse to the WDNCRL_Rev18.03

folder and double-click the index.html to open the guide in your default

browser.

#####

 

The download link for RTA is:

https://nxp-be-prod.zoominsoftware.io/bundle/GUID-487B2E69-BB19-42CB-AC38-7E

F18C0FE3AE/page/GUID-D6A87248-D5A0-43B8-9AC4-69D3FF39D5A3.zip

The download link for RTA  document in PDF is:

https://nxp-be-prod.zoominsoftware.io/bundle/GUID-487B2E69-BB19-42CB-AC38-7E

F18C0FE3AE/page/GUID-B4854EB7-7296-4C52-B28E-3E3456C4F9F6.pdf

 

Customer will able to find the reference and use cases of SEC engine in

LSDK's IPsec, openssl, DPDK, cryptodev, and uboot code.

 

For secure boot, software procedure is in LSDK User Guide, e.g.

https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/G

UID-65A50152-786D-4579-BA20-A540495AD735.html

The registers level detail is in a NDA document, "QorIQ Trust Architecture

2.1 User Guide". Customer need separate request to access it from the Trust

Architecture User group.

 

0 件の賞賛
返信

4,191件の閲覧回数
roger_davis
Contributor II

Only one link out of these works. The others go to page not found.

0 件の賞賛
返信

4,182件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

4,207件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The RTIC is documented in the LS1046ASECRM.pdf, which can be download from

the nxp.com. Please refers to

Chapter 12 Trust Architecture modules

12.1 Run-time integrity checker

(RTIC)......................................................................

.......................................................651

12.1.1 RTIC modes of

operation...................................................................

........................................................651

12.1.2 RTIC initialization and

operation...................................................................

........................................... 651

12.1.3 RTIC use of the Throttle

Register....................................................................

..........................................652

12.1.4 RTIC use of command, configuration, and status

registers...................................................................

.... 652

12.1.5 Initializing

RTIC........................................................................

................................................................ 653

12.1.6 RTIC Memory Block Address/Length

Registers...................................................................

....................653

 

There are no C level source code samples for it. To run a demo, customer can

touch the registers to enable it. Here are the sample procedures in uboot

with registers level configuration.

#####

Run time integrity checker (RTIC) is a hardware feature that checks the

integrity of the operating environment. You can use RTIC to monitor binary

images, set it up as a static data area, or administrative database that are

constant in nature. As soon as RTIC detects any modification in the memory

regions it monitors, you can either send an interpretation to the host for

post processing, or change the security state of the SoC to lockout

cryptographic key(s) access to protect sensitive date.

 

Below is a register level prototype to enable RTIC to monitor a pre-defined

memory region.

=> mw.l a0000000 11112222 100  <-# init RAM address

=> md 0x1760000 4        <-display RTIC status

01760000: 00000000 00000400 00000000 00000000    ................

=> mw.l 0x176001c 0xff000000     <- # set RTIC Throttle (RTHR)

=> mw.l 0x176002c 0xffff0000       <- # set RTIC Watchdog Timer (RWDOG)

=> mw.l 0x1760104 000000a0       <- # set RTIC monitor address (RMAA)

=> mw.l 0x176010c 00010000        <- # set RTIC monitor length (RMAL)

=> mw.l 0x1760014 10010000       <- Enable and unlock run time memory (RCTL)

=> mw.l 0x176000c 02000000        <- Hash block A once (RMAL)

=> mw.l 0x176000c 04000000        <- Enable Run Time Check (RMAL)

=> md 0x1760000; md 0x1760000 <- display RTIC Status (RSTA)

01760000: 00000000 01000004 00000000 00000000    ................

01760000: 00000000 01000a04 00000000 00000000    ................

01 = RTIC Busy, 02 = Hash Once Operation Completed. 04=sec violation

00 = no address error for all four blocks

0a = RTD, RTIC is in Run Time mode, All blocks hashed (ABH)

04 = run time state, 02 Single Hash State, 06 = Error State

When the RTIC monitored memory region is modified, the SECMON changes the

state to non-secure and locks out black key access for further cryptographic

operations.

=> md 0x1760000; echo; md 01e90000;

01760000: 00000000 01000004 00000000 00000000    ................

01760010: 00000000 10110000 00000000 ff000000    ................

 

01e90000: 00000000 00000000 00000000 00000000    ................

01e90010: 00000000 00ad0080 00000000 00000000    ................  <-

Trusted state, OTPMK programmed

=> mw.l a0000000 01234567                  <- modify any area monitored

by RTIC block A

=> md 0x1760000; echo; md 01e90000;                <- take few cycles for RTIC

to update state!

01760000: 00000000 14000206 00000000 00000000    ................

01760010: 00000000 10100000 00000000 ff000000    ................

 

01e90000: 00000000 00000000 00000000 00000000    ................

01e90010: 00000000 00a30088 01000000 00000000    ................ <- HPSR:

SSM = Soft fail.OTPMK=0

Recall for the SecMon_HP Status register (HPSR), 0x88 means both OPTMK and

ZMK, and 0x03 means that the security monitor is in a soft fail state.

#####

0 件の賞賛
返信