SEC Initialization in Trusted State

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SEC Initialization in Trusted State

1,805件の閲覧回数
shivesh_sood
Contributor I

Hi,

We are running a custom bootloader on our LS1046ARDB - The code performs authentication of an image and passes control. With SB_EN disabled in RCW and the system in SECMON in Check State, the SEC is initialized successfully and can process jobs through the Job Ring Interface. However, when we enable secure boot and execute the same boot code with SECMON in Trusted State, the SEC is not getting initialized and any jobs passed through input JR gives an error code 0x13 (DECO Source) in JRSTAR_JR0 register [ Header Error (Invalid length or parity, or certain other problems.) ]

What could be the reason here - are we missing some key differences in SEC behavior and initialization steps when Secure Boot is enabled vs. when Secure Boot is Disabled? 

Thanks,

@chitra_amzarewa 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,794件の閲覧回数
bpe
NXP Employee
NXP Employee

To provide detailed comments to this post, I may need to share information available only under NDA, which is not possible on a public Forum. Consider opening a Support Case

Best Regards,
Platon

 

0 件の賞賛
返信

1,779件の閲覧回数
shivesh_sood
Contributor I

Done. Thank you

0 件の賞賛
返信