SEC Initialization in Trusted State

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEC Initialization in Trusted State

1,804 Views
shivesh_sood
Contributor I

Hi,

We are running a custom bootloader on our LS1046ARDB - The code performs authentication of an image and passes control. With SB_EN disabled in RCW and the system in SECMON in Check State, the SEC is initialized successfully and can process jobs through the Job Ring Interface. However, when we enable secure boot and execute the same boot code with SECMON in Trusted State, the SEC is not getting initialized and any jobs passed through input JR gives an error code 0x13 (DECO Source) in JRSTAR_JR0 register [ Header Error (Invalid length or parity, or certain other problems.) ]

What could be the reason here - are we missing some key differences in SEC behavior and initialization steps when Secure Boot is enabled vs. when Secure Boot is Disabled? 

Thanks,

@chitra_amzarewa 

Labels (1)
0 Kudos
Reply
2 Replies

1,793 Views
bpe
NXP Employee
NXP Employee

To provide detailed comments to this post, I may need to share information available only under NDA, which is not possible on a public Forum. Consider opening a Support Case

Best Regards,
Platon

 

0 Kudos
Reply

1,778 Views
shivesh_sood
Contributor I

Done. Thank you

0 Kudos
Reply