SDK LS1043 doesn't have /usr/local/lib in filesys after adding python-dev

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK LS1043 doesn't have /usr/local/lib in filesys after adding python-dev

1,726 次查看
tracysmith
Contributor IV

Refer to SDK LS1043 doesn't have /usr/include/.../Python.h in filesys? 

After adding IMAGE_INSTALL_append = " python-dev" to layer.conf in ./sources/meta-openembedded/meta-python/conf, Python.h is included in /usr/include/python2.7/Python.h, but python libraries are now under /usr/lib instead of /usr/local/lib.  There is no longer a /usr/local after adding the IMAGE_INSTALL_append = " python-dev" to layer.conf.

Having trouble with the python library location and path after adding the SDK 2.0 python-dev package.  After adding the python-dev package, the sys.path changes from /usr/local/lib to /usr/lib and places python libraries into /usr/lib instead of /usr/local/lib breaking build bot that uses python on the LS1043A where the tools use /usr/local/lib instead of /usr/lib. 

Why is this and how can we indicate where to place the python-dev package on the rootfs using recipes?

 

How can we modify rootfs to place any needed libraries under /usr/local/lib and how can sys.path be changed as needed for the rootfs?

 

Thx,

Tracy

 

The base path difference, original path is /usr/lib vs /usr/local/lib after adding python-dev. Why and how can this be avoided using the rootfs python-dev .bb file(s)?

 

LS1043A ROOTFS AFTER ADDING PYTHON DEV PACKAGE

 

>>> print("\n".join(sys.path))

/usr/lib/python27.zip
/usr/lib/python2.7
/usr/lib/python2.7/plat-linux2
/usr/lib/python2.7/lib-tk
/usr/lib/python2.7/lib-old
/usr/lib/python2.7/lib-dynload
/usr/lib/python2.7/site-packages
/usr/lib/python2.7/site-packages/newrelic-2.22.0.19
/usr/lib/python2.7/site-packages/setuptools-18.2-py2.7.egg

LS1043A ROOTFS BEFORE ADDING PYTHON DEV PACKAGE

>>> print("\n".join(sys.path))

/usr/local/lib/python27.zip
/usr/local/lib/python2.7
/usr/local/lib/python2.7/plat-linux2
/usr/local/lib/python2.7/lib-tk
/usr/local/lib/python2.7/lib-old
/usr/local/lib/python2.7/lib-dynload
/usr/local/lib/python2.7/site-packages

 

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,467 次查看
tracysmith
Contributor IV

Hi Yiping,

I have added the bb file after adding the dev-python package.  Do you see anything causing the behavior or any other changes that might be needed in the recipe?

thx,

Tracy

0 项奖励
回复

1,467 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tracy Smith,

I check the fsl-image-core rootfs provided in SDK 2.0 prebuilt image ISO, python2.7 folder is located in /usr/lib/, the same path as python-dev package libraries deployed.

In the recipe sources/poky/meta/recipes-devtools/python/python_2.7.9.bb, the variable STAGING_LIBDIR used in the Makefile of python package is defined as /usr/lib in Yocto by default.

I am not sure why you got python libraries deployed in /usr/local, I suspect whether you used the same python recipe as I mentioned above.

Would you please recover your original build environment and run the command "bitbake python-dev -c patch -f" to get which python recipe is used from the building log?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,467 次查看
tracysmith
Contributor IV

Working on getting details requested. Please don't close.  Engineer on vacation until Monday so it may be sometime next week before being able to reply.

0 项奖励
回复