SDK 2.0 How to build and add RT-Tests package in yocto for rootfs?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK 2.0 How to build and add RT-Tests package in yocto for rootfs?

2,149 次查看
pro-supportengi
NXP Employee
NXP Employee

The document below has the following:

RT-tests suit contains various test applications like cyclictest, hackbench, etc to measure latencies and induce various test loads.

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-5E34A886-778F-470E-8C9B-5...

How do we build the RT-tests as a package in yocto and build it into the rootfs?  We do not see a package for the RT patch supported for local.conf when building.  What enables the Yocto RT-test package in yocto?

Also, can it be built for both the core and full image builds?

Also it should be noted, PREEMPT_RT has been validated on the LS1043ARDB by NXP.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,753 次查看
bpe
NXP Employee
NXP Employee

The name of the SDK package that contains rt tests is 'rt-tests'

The article at the URL below describes how to add packages to the rootfs:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-F077305B-5163-44EA-A9B0-3...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复