SD Clock source is not correct in LS1046

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD Clock source is not correct in LS1046

1,742件の閲覧回数
charleshuang
Senior Contributor II

Hi NXP Team

My platform follow the LS1046ardb demo board.

I try to test  "boot form SD card", but I can not boot form SD.

(1) In Demo board The CLK1 = 156Mhz

charleshuang_1-1638951463351.png

(2) In my design board CLK1 =100Mhz

charleshuang_0-1638951441007.png

Why the CLK1 is different, my source code the same with Demoboard.

Do you have any advice?

The CLK1 is not correct.  I can not boot up form SD, right?

ラベル(2)
0 件の賞賛
返信
1 返信

1,732件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following in checkboard function in board/freescale/ls1046ardb/ls1046ardb.c in u-boot source code.

int checkboard(void)
{
static const char *freq[2] = {"100.00MHZ", "156.25MHZ"};

......

puts("SERDES Reference Clocks:\n");
sd1refclk_sel = CPLD_READ(sd1refclk_sel);
printf("SD1_CLK1 = %s, SD1_CLK2 = %s\n", freq[sd1refclk_sel], freq[0]);

return 0;
}

The value of sd1refclk_sel is read from CPLD, however you didn't program CPLD firmware on your target board, so the variable sd1refclk_sel is 0, SD1_CLK1( freq[sd1refclk_sel]) is freq[0], it is 100MHZ.

So, please program CPLD and FPGA on your custom board.

0 件の賞賛
返信