Run /sbin/init as init process Unable to handle kernel paging request at virtual address 0040326054

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run /sbin/init as init process Unable to handle kernel paging request at virtual address 0040326054

ソリューションへジャンプ
4,235件の閲覧回数
Hugh512
Contributor III

My board is based on ls1012ardb, my sdk is lsdk2108.

My NOR flash layout is:
[ 2.310553] 0x000000000000-0x000000100000 : "pbl"
[ 2.323334] 0x000000100000-0x000000280000 : "uboot"
[ 2.335312] 0x000000280000-0x0000002c0000 : "uboot-env"
[ 2.347304] 0x0000002c0000-0x000000fc0000 : "kernel"
[ 2.359308] 0x000001000000-0x000001c00000 : "rootfs"
[ 2.371346] 0x000001c00000-0x000002000000 : "data"

boot args is:
set bootargs console=ttyS0,115200 noinitrd root=/dev/mtdblock4 rootfstype=squashfs rootwait rw earlycon=uart8250,mmio,0x21c0500 quiet lpj=250000

The rootfs is built by command "flex-builder -i mkrfs -r yocto:tiny"

[ 3.259000] VFS: Mounted root (squashfs filesystem) readonly on device 31:4.
[ 3.267769] devtmpfs: mounted
[ 3.276036] Freeing unused kernel memory: 6656K
[ 3.280714] Run /sbin/init as init process
[ 3.284858] with arguments:
[ 3.287836] /sbin/init
[ 3.290542] with environment:
[ 3.293705] HOME=/
[ 3.296074] TERM=linux
INIT: version 2.99 booting
INIT: /etc/inittab[32]: missing id field
[ 3.751928] Unable to handle kernel paging request at virtual address 00403260540003e1
[ 3.760040] Mem abort info:
[ 3.762861] ESR = 0x96000004
[ 3.765917] EC = 0x25: DABT (current EL), IL = 32 bits
[ 3.771265] SET = 0, FnV = 0
[ 3.774322] EA = 0, S1PTW = 0
[ 3.777473] Data abort info:
[ 3.780378] ISV = 0, ISS = 0x00000004
[ 3.784226] CM = 0, WnR = 0
[ 3.787204] [00403260540003e1] address between user and kernel address ranges
[ 3.794375] Internal error: Oops: 96000004 [#1] PREEMPT SMP
[ 3.799956] Modules linked in:
[ 3.803022] CPU: 0 PID: 121 Comm: pidof Not tainted 5.10.35-00002-gd06856fba47f-dirty #10
[ 3.811213] Hardware name: LS1012A RDB Board (DT)
[ 3.815925] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--)
[ 3.821949] pc : wq_worker_comm+0x78/0xd0
[ 3.825964] lr : wq_worker_comm+0x78/0xd0
[ 3.829977] sp : ffff800012f9ba60
[ 3.833294] x29: ffff800012f9ba60 x28: ffff800010122a60
[ 3.838619] x27: ffffffffffffffff x26: ffff0000017800c0
[ 3.843943] x25: 0000000000000127 x24: 0000000000000000
[ 3.849267] x23: ffff800012f9bae8 x22: ffff8000124f0fb8
[ 3.854592] x21: 000000000000000c x20: 0000000000000040
[ 3.859916] x19: ffff0000010c4040 x18: 0000000000001000
[ 3.865240] x17: 0000000000000000 x16: 0000000000000000
[ 3.870564] x15: ffff000001780520 x14: 0000000000000001
[ 3.875888] x13: ffff800012f9bad0 x12: 0000000000000010
[ 3.881212] x11: 0101010101010101 x10: 7f7f7f7f7f7f7f7f
[ 3.886536] x9 : ffff800012f9baf0 x8 : fefefefefefefeff
[ 3.891859] x7 : 0000000000000040 x6 : ffff800012f9bae8
[ 3.897184] x5 : 000000006574656c x4 : 0000000000000000
[ 3.902507] x3 : ffff8000124f0fb8 x2 : ffff0000017800c0
[ 3.907830] x1 : 0000000004208060 x0 : b9403260540003a1
[ 3.913155] Call trace:
[ 3.915604] wq_worker_comm+0x78/0xd0
[ 3.919273] proc_task_name+0x4c/0x138
[ 3.923028] do_task_stat+0x358/0xa38
[ 3.926693] proc_tgid_stat+0x14/0x20
[ 3.930359] proc_single_show+0x5c/0x110
[ 3.934291] seq_read_iter+0x258/0x460
[ 3.938045] seq_read+0xdc/0x130
[ 3.941277] vfs_read+0xac/0x1d8
[ 3.944507] ksys_read+0x6c/0x100
[ 3.947826] __arm64_sys_read+0x1c/0x28
[ 3.951670] el0_svc_common.constprop.0+0x78/0x1a0
[ 3.956470] do_el0_svc+0x24/0x90
[ 3.959791] el0_svc+0x14/0x20
[ 3.962846] el0_sync_handler+0xb0/0xb8
[ 3.966687] el0_sync+0x178/0x180
[ 3.970010] Code: d50323bf d65f03c0 aa1303e0 940010c1 (f9402018)
[ 3.976115] ---[ end trace ca17af90850baae9 ]---
Segmentation fault
Starting udev
[ 4.050720] Unable to handle kernel paging request at virtual address 0040d3f37bc2312c
[ 4.058676] Mem abort info:
[ 4.061471] ESR = 0x96000004
[ 4.064537] EC = 0x25: DABT (current EL), IL = 32 bits
[ 4.069864] SET = 0, FnV = 0
[ 4.072928] EA = 0, S1PTW = 0
[ 4.076078] Data abort info:
[ 4.078967] ISV = 0, ISS = 0x00000004
[ 4.082819] CM = 0, WnR = 0
[ 4.085788] [0040d3f37bc2312c] address between user and kernel address ranges
[ 4.092945] Internal error: Oops: 96000004 [#2] PREEMPT SMP
[ 4.098526] Modules linked in:
[ 4.101590] CPU: 0 PID: 94 Comm: kworker/0:2 Tainted: G D 5.10.35-00002-gd06856fba47f-dirty #10
[ 4.111609] Hardware name: LS1012A RDB Board (DT)
[ 4.116333] Workqueue: events linkwatch_event
[ 4.120698] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--)
[ 4.126717] pc : linkwatch_do_dev+0x5c/0xf0
[ 4.130907] lr : linkwatch_do_dev+0xa4/0xf0
[ 4.135095] sp : ffff800012e1bce0
[ 4.138412] x29: ffff800012e1bce0 x28: ffff00000118e000
[ 4.143737] x27: ffff80001279fa48 x26: ffff000000254140
[ 4.149061] x25: ffff8000128c1e68 x24: 0000000000000000
[ 4.154385] x23: ffff8000128c1e78 x22: ffff800012e1bd68
[ 4.159709] x21: ffff80001279f9f0 x20: 0000000000000064
[ 4.165033] x19: ffff00000118e000 x18: 0000000000001000
[ 4.170357] x17: 0000000000000000 x16: 0000000000000000
[ 4.175681] x15: 00008e27a6679cae x14: 00000000000003cd
[ 4.181005] x13: 00000000000003cd x12: 0000000000005db1
[ 4.186329] x11: 071c71c71c71c71c x10: 00000000000009c0
[ 4.191653] x9 : ffff00000108b76c x8 : fefefefefefefeff
[ 4.196976] x7 : 0000000000000018 x6 : ffff00000108b76c
[ 4.202300] x5 : 000073746e657665 x4 : 0000000000000000
[ 4.207625] x3 : 00000000ffffffff x2 : ffff800027c23000
[ 4.212949] x1 : ffff000000254140 x0 : a940d3f37bc2312c
[ 4.218273] Call trace:
[ 4.220723] linkwatch_do_dev+0x5c/0xf0
[ 4.224565] __linkwatch_run_queue+0xe0/0x218
[ 4.228930] linkwatch_event+0x2c/0x40
[ 4.232686] process_one_work+0x1bc/0x338
[ 4.236700] worker_thread+0x50/0x420
[ 4.240367] kthread+0x154/0x158
[ 4.243598] ret_from_fork+0x10/0x34
[ 4.247181] Code: 12800003 d538d082 f9426260 8b020000 (885f7c05)
[ 4.253286] ---[ end trace ca17af90850baaea ]---
[ 4.257931] note: kworker/0:2[94] exited with preempt_count 1
[ 8.306704] Unable to handle kernel paging request at virtual address 00030021d0000417
[ 8.314660] Mem abort info:
[ 8.317463] ESR = 0x96000004
[ 8.320529] EC = 0x25: DABT (current EL), IL = 32 bits
[ 8.325856] SET = 0, FnV = 0
[ 8.328920] EA = 0, S1PTW = 0
[ 8.332069] Data abort info:
[ 8.334959] ISV = 0, ISS = 0x00000004
[ 8.338804] CM = 0, WnR = 0
[ 8.341773] [00030021d0000417] address between user and kernel address ranges
[ 8.348928] Internal error: Oops: 96000004 [#3] PREEMPT SMP
[ 8.354508] Modules linked in:
[ 8.357574] CPU: 0 PID: 70 Comm: kworker/0:1H Tainted: G D 5.10.35-00002-gd06856fba47f-dirty #10
[ 8.367680] Hardware name: LS1012A RDB Board (DT)
[ 8.372399] Workqueue: kblockd blk_mq_timeout_work
[ 8.377203] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--)
[ 8.383221] pc : blk_mq_queue_tag_busy_iter+0xc0/0x340
[ 8.388368] lr : blk_mq_queue_tag_busy_iter+0x2d0/0x340
[ 8.393597] sp : ffff800012b4bca0
[ 8.396914] x29: ffff800012b4bca0 x28: ffff8000124d6000
[ 8.402239] x27: ffff0000003ee5c8 x26: ffff8000127d7a08
[ 8.407563] x25: 0000000000000000 x24: ffff0000011e17c0
[ 8.412887] x23: fffffdffbffdf000 x22: ffff0000011e17c0
[ 8.418211] x21: 91030021d0000321 x20: 0000000000000000
[ 8.423535] x19: ffff0000011e1b70 x18: 000000000000000e
[ 8.428859] x17: 0000000000000001 x16: 0000000000000019
[ 8.434183] x15: 0000000000000000 x14: 00000000000000d7
[ 8.439507] x13: 0000000000000000 x12: 0000000000000000
[ 8.444831] x11: 0000000000000000 x10: 00000000000009c0
[ 8.450155] x9 : ffff0000003e336c x8 : fefefefefefefeff
[ 8.455479] x7 : 0000000000000018 x6 : ffff0000003e336c
[ 8.460803] x5 : 0000000000000002 x4 : 0000000000000000
[ 8.466126] x3 : 0000000000000001 x2 : ffff800027c23000
[ 8.471450] x1 : 0000000000000001 x0 : ffff000001181700
[ 8.476773] Call trace:
[ 8.479225] blk_mq_queue_tag_busy_iter+0xc0/0x340
[ 8.484022] blk_mq_timeout_work+0x144/0x1a8
[ 8.488298] process_one_work+0x1bc/0x338
[ 8.492312] worker_thread+0x50/0x420
[ 8.495980] kthread+0x154/0x158
[ 8.499212] ret_from_fork+0x10/0x34
[ 8.502794] Code: 6b14003f 540005a9 f9402700 f874d815 (7941eea0)
[ 8.508898] ---[ end trace ca17af90850baaeb ]---

ラベル(1)
0 件の賞賛
返信
1 解決策
4,198件の閲覧回数
Hugh512
Contributor III

Dear Chavira:
Thanks for helping. The rootfs is built by command "flex-builder -i mkrfs -r yocto:tiny" , it is not work for me. Finally, I make rootfs from busybox. It works for me.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,223件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

If your board is based on LS1012ARDB, please install the pre-compiled image on your board and try to boot.

We have a manual to deploy images to different devices that you can boot, please read that manual for your boot type.

Flash Bank Usage | QorIQ SDK v2.0-1703 Documentation | NXP Semiconductors

0 件の賞賛
返信
4,199件の閲覧回数
Hugh512
Contributor III

Dear Chavira:
Thanks for helping. The rootfs is built by command "flex-builder -i mkrfs -r yocto:tiny" , it is not work for me. Finally, I make rootfs from busybox. It works for me.

0 件の賞賛
返信