Real-time Edge Software on LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Real-time Edge Software on LS1046A

1,451件の閲覧回数
Chanh
Contributor III

Hi,

I have an LS1046AFRWY board and I want to try Real-time Edge Software, I have few questions on it:

  1. From "Table 3. Key features", seems bare metal is not supported for LS1046AFRWY, but supported for LS1046ARDB, may I know why there is a different? As suppose the hardware is almost similar.

  2. Also from this table, GPIO under bare metal is not supported. Does it mean bare metal cannot access to GPIO? and why?

Thanks.

0 件の賞賛
返信
1 返信

1,426件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

1. You could add  LS1046AFRWY bare mental by yourself, please refer to configs/ls1046ardb_bm_defconfig in source code to create the configuration file for LS1046AFRWY.

2. GPIO can be supported, please refer to the source code for i.MX 8MM, 8MP or LS1021A-IoT.

0 件の賞賛
返信