Question Regarding TSN Configuration on LS1028a?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question Regarding TSN Configuration on LS1028a?

Jump to solution
1,647 Views
LedHx
Contributor II

Hello,

I am currently working on secondary development related to TSN using the LS1028A platform. In the manual, I noticed that the tsntool is recommended for configuring TSN-related features. I would like to know if there are alternative methods to configure TSN without using tsntool. For example, can I directly manipulate the enetc driver for configuration? If so, is there any documentation available for the driver?

Thank you.

Tags (1)
0 Kudos
Reply
1 Solution
1,585 Views
June_Lu
NXP TechSupport
NXP TechSupport

Direct configuration through Linux is not supported, please kindly use the tsntool.

Thanks

View solution in original post

3 Replies
1,570 Views
June_Lu
NXP TechSupport
NXP TechSupport

Confirmed by the internal team, yes, it's correct.

0 Kudos
Reply
1,586 Views
June_Lu
NXP TechSupport
NXP TechSupport

Direct configuration through Linux is not supported, please kindly use the tsntool.

Thanks

1,582 Views
LedHx
Contributor II
That is to say, during secondary development, I can only either call this tool within my own code or reference its source code in my project. Is that correct?
0 Kudos
Reply