QorIQ-SDK-V2.0 no openjdk, can't build java-test-image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ-SDK-V2.0 no openjdk, can't build java-test-image

1,353 Views
steffendedekind
Contributor II

Hello,

currently I want to use the LS1043ARDB for some testing. So I downloaded the newest (?) SDK:

QorIQ-SDK-V2.0

And start building some images: fsl-image-minimal, fsl-image-core, fsl-image-full, fsl-image-kernelitb anything works fine so far. But for our automated target testing I need java for (Hudson/Jenkins) and I tried to build the java-test-image for this.

It seems like openjdk (or jdk at all) support has been removed - I'm not sure if this is intended or if only the needed recepies are missing.

sd@sd-VirtualBox:~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb$ bitbake java-test-image
Loading cache: 100% |########################################################################################################################################################################| ETA: 00:00:00
Loaded 3421 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'openjdk-7-jre' (but /home/sd/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-java/recipes-images/images/java-test-image.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'openjdk-7-jre' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['openjdk-7-jre']
ERROR: Required build target 'java-test-image' has no buildable providers.
Missing or unbuildable dependency chain was: ['java-test-image', 'openjdk-7-jre']

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
sd@sd-VirtualBox:~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb$

Any suggestions/solutions ?

#ls1043a#qoriq sdk 2#java

Labels (1)
0 Kudos
Reply
1 Reply

1,054 Views
Pavel
NXP Employee
NXP Employee

This feature does not work on the SDK 2.0.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply