QUADSPI boot initialization sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QUADSPI boot initialization sequence

937 次查看
pelegk
Contributor I

 

hello,

in my application, i will use the LS1023 MPU.

I would like to use the QUADSPI boot initialization, which means that in Power on, the image will be taken from NOR flash in QSPI.

in chapter 4.4.5.1 note 2, is written that Booting from QSPI takes precedence , when mentioned QSPI A.

my question is, if QuadSPI boot initialization sequence demends QSPI A only, or can i use the QSPI B.

if its possible to boot from QSPI B, my next question is how the MPU knows from which channel to take the image.

your advise please

peleg

标签 (1)
0 项奖励
回复
1 回复

931 次查看
ufedor
NXP Employee
NXP Employee

> is written that Booting from QSPI takes precedence

The note is about pin multiplexing and means that mentioned QSPI signals' functions will be configured forcibly if QuadSPI is selected as RCW source.

 

Booting is possible only from QSPI_A.

0 项奖励
回复