Problems with lsdk2004 kernel 5.4 HW Timestamping

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems with lsdk2004 kernel 5.4 HW Timestamping

1,481 次查看
540915622
Contributor III

Refer to LSDKUG_Rev20.04_290520.pdf for the following operations, but the same result cannot be obtained。

pastedImage_2.png

All application components have been compiled into the file system。

pastedImage_3.png

How to start tsn network using lsdk2004 on ls1028ardb, what configuration needs to be done on the kernel.

0 项奖励
回复
1 回复

1,412 次查看
bpe
NXP Employee
NXP Employee

Based on your console outputs, your kernel is missing FSL_ENETC_HW_TIMESTAMPING option. Make sure this option is

set to "Y" and rebuild. See LSDK UM Section 8.7.1.2 for more information.


Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复