Problem in using the Flash Programmer of CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in using the Flash Programmer of CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.7

Jump to solution
2,851 Views
nagireddychitta
Contributor III

Hi,

I am using TWR-LS1021A-PB evolution board and trying to use Flash Programmer which is part of CW Dev Studio(Version:10.0.7) to Flash the UBoot in NOR Flash Bank1 area of EV Board, but seems like Erase is working but not program.

I have chosen the "Flash File To Target" Option from Flash Programmer ikon and followed the steps according to the help provided by Freescale.

Pls see the Console output when i execute the Target Task.

/////////////////////////////////////////////////////////////////////////////////////////////////

fl::target -lc "LC for Simple Flash"

fl::target -b 0x10000000 0x20000

fl::target -v off -l off

cmdwin::fl::device -d "JS28F00AM29EWHA" -o "64Mx16x1" -a 0x60000000 0x67ffffff

cmdwin::fl::image -f "F:\\Debug\\u-boot\\u-boot.bin" -t "Auto Detect" -re on -r 0x60000000 0x67ffffff -oe on -o 0x4100000

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

Image size is 0 bytes, nothing to erase.  

Nothing to erase.  No sectors selected

Performing target initialization ...   

     1570200  <m>0xFFFFFFFF</m>   .... 

Erase Command Succeeded.  

cmdwin::fl::write

-------------------------

Using restricted address range 0x60000000 to 0x67FFFFFF  

Programming file F:\Debug\u-boot\u-boot.bin  

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

0 Bytes Programmed, Check Restricted Address Range  

Program Command Succeeded

/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Does anyone in the community tried this on the LS1021A Evo board?

I would really appreciate for any help to fix this issue.

Best Regards,

Nagi

Labels (1)
0 Kudos
Reply
1 Solution
2,709 Views
nagireddychitta
Contributor III

Hi Adrian,

That is right indeed.

Regards,

Nagi

View solution in original post

0 Kudos
Reply
2 Replies
2,709 Views
addiyi
NXP Employee
NXP Employee

From the log it seems that offset address is not in the address range. For uboot, it should be something like 0x60100000 (depending on the rcw used).

Adrian

0 Kudos
Reply
2,710 Views
nagireddychitta
Contributor III

Hi Adrian,

That is right indeed.

Regards,

Nagi

0 Kudos
Reply