Problem in using the Flash Programmer of CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in using the Flash Programmer of CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.7

ソリューションへジャンプ
2,852件の閲覧回数
nagireddychitta
Contributor III

Hi,

I am using TWR-LS1021A-PB evolution board and trying to use Flash Programmer which is part of CW Dev Studio(Version:10.0.7) to Flash the UBoot in NOR Flash Bank1 area of EV Board, but seems like Erase is working but not program.

I have chosen the "Flash File To Target" Option from Flash Programmer ikon and followed the steps according to the help provided by Freescale.

Pls see the Console output when i execute the Target Task.

/////////////////////////////////////////////////////////////////////////////////////////////////

fl::target -lc "LC for Simple Flash"

fl::target -b 0x10000000 0x20000

fl::target -v off -l off

cmdwin::fl::device -d "JS28F00AM29EWHA" -o "64Mx16x1" -a 0x60000000 0x67ffffff

cmdwin::fl::image -f "F:\\Debug\\u-boot\\u-boot.bin" -t "Auto Detect" -re on -r 0x60000000 0x67ffffff -oe on -o 0x4100000

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

Image size is 0 bytes, nothing to erase.  

Nothing to erase.  No sectors selected

Performing target initialization ...   

     1570200  <m>0xFFFFFFFF</m>   .... 

Erase Command Succeeded.  

cmdwin::fl::write

-------------------------

Using restricted address range 0x60000000 to 0x67FFFFFF  

Programming file F:\Debug\u-boot\u-boot.bin  

Auto-detection is successful.  

  File is of type Binary/Raw Format.  

0 Bytes Programmed, Check Restricted Address Range  

Program Command Succeeded

/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Does anyone in the community tried this on the LS1021A Evo board?

I would really appreciate for any help to fix this issue.

Best Regards,

Nagi

ラベル(1)
0 件の賞賛
返信
1 解決策
2,710件の閲覧回数
nagireddychitta
Contributor III

Hi Adrian,

That is right indeed.

Regards,

Nagi

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,710件の閲覧回数
addiyi
NXP Employee
NXP Employee

From the log it seems that offset address is not in the address range. For uboot, it should be something like 0x60100000 (depending on the rcw used).

Adrian

0 件の賞賛
返信
2,711件の閲覧回数
nagireddychitta
Contributor III

Hi Adrian,

That is right indeed.

Regards,

Nagi

0 件の賞賛
返信